CMP#.MODEN

Description

CMP#.MODEN turns the modulo function for the compare channel on or off.

Examples

Usage

0: Turn modulo off (default)

1: Turn modulo on

Code

The following commands turn modulo on for channel 1 and off for channel 2.

--> CMP1.MODEN 1
--> CMP2.MODEN 0

Context

For more information please refer to Compare.

Versions

Action Version Notes
Implemented 02-06-00-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

CMP#.MODVAL1, CMP#.MODVAL2

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.